• AVR Freaks

Hot!urgent trouble with MPLAB-x IDE

Author
jjros
New Member
  • Total Posts : 4
  • Reward points : 0
  • Joined: 2020/06/20 00:46:16
  • Location: 0
  • Status: offline
2020/06/30 11:05:28 (permalink)
3 (2)

urgent trouble with MPLAB-x IDE

hi, in mplab-IDE i have a trouble,
at project create the step1 is correct, but,
al step2 appears 'Target location' instead of select processor.
I don't understand what the problem is,
I have installed mplab-x at least four times even as administrator,
I need help, thanks.

Attachment(s)

Attachments are not available: Download requirements not met
#1

2 Replies Related Threads

    PStechPaul
    Super Member
    • Total Posts : 2807
    • Reward points : 0
    • Joined: 2006/06/27 16:11:32
    • Location: Cockeysville, MD, USA
    • Status: offline
    Re: urgent trouble with MPLAB-x IDE 2020/06/30 13:44:25 (permalink)
    +1 (1)
    Maybe you need to give the project a name first, and the select the processor?

     
    #2
    RISC
    Super Member
    • Total Posts : 5772
    • Reward points : 0
    • Status: online
    Re: urgent trouble with MPLAB-x IDE 2020/06/30 14:19:39 (permalink)
    0
    Hi,
    there are lots of tutorials to get started with MPLAB X here : https://microchipdeveloper.com
    Regards

    For support make sure to check first here : http://microchipdeveloper.com
    There are hundreds of PIC, AVR, SAM...which one do YOU use ?
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5