• AVR Freaks

Hot!On New Project in step 2 i have "..." target location what i can do ?

Author
Асем
New Member
  • Total Posts : 2
  • Reward points : 0
  • Joined: 2020/06/20 11:31:17
  • Location: 0
  • Status: offline
2020/06/27 08:31:50 (permalink)
0

On New Project in step 2 i have "..." target location what i can do ?

Hello guys 

Attached Image(s)

#1

2 Replies Related Threads

    du00000001
    Just Some Member
    • Total Posts : 3850
    • Reward points : 0
    • Joined: 2016/05/03 13:52:42
    • Location: Germany
    • Status: offline
    Re: On New Project in step 2 i have "..." target location what i can do ? 2020/06/29 08:32:48 (permalink)
    0
    Hope you already round out - e.g. by reading some of the documentation supplied:
    the poor target needs a "home" - - - which is expected to be provided here.

    PEBKAC / EBKAC / POBCAK / PICNIC (eventually see en.wikipedia.org)
    #2
    ric
    Super Member
    • Total Posts : 28006
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: offline
    Re: On New Project in step 2 i have "..." target location what i can do ? 2020/06/29 15:39:29 (permalink)
    5 (1)
    In other words, it is YOUR job to tell MPLABX where you want the project saved on your computer.
    Select a folder.
    Just be aware, MOST MPLABX tools support long filenames, but there always seems to be one step that throws up if your path contains non-ASCII characters.
     
     

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5