• AVR Freaks

Hot!Harmony V2 , PIC32MX / external flash IC programming through USB from PC

Author
JEGANATH
New Member
  • Total Posts : 6
  • Reward points : 0
  • Joined: 2020/03/27 23:53:38
  • Location: 0
  • Status: offline
2020/06/26 04:46:58 (permalink)
0

Harmony V2 , PIC32MX / external flash IC programming through USB from PC

I'm using PIC32MX795F512L custom board with  external flash  IC (W25Q128FV), i need to load 15MB Bin file into flash IC  from my PC through USB.
Can I use Harmony CDC_COM_PORT_SINGLE demo for programming the flash IC ?
post edited by JEGANATH - 2020/06/26 19:30:47
#1

1 Reply Related Threads

    ric
    Super Member
    • Total Posts : 28006
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: online
    Re: Harmony V2 , PIC32MX / external flash IC programming through USB from PC 2020/06/26 20:14:06 (permalink)
    0
    Duplicate of https://www.microchip.com/forums/m1145495.aspx
    Please stick to the first topic.

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #2
    Jump to:
    © 2020 APG vNext Commercial Version 4.5