• AVR Freaks

Hot!RE: parallel flash driver interfaceable with pmp port of dspic33ep

Author
Rabi
Embedded engineer
  • Total Posts : 9
  • Reward points : 0
  • Joined: 2020/05/14 23:49:25
  • Location: 0
  • Status: offline
2020/06/24 08:19:01 (permalink)
0

RE: parallel flash driver interfaceable with pmp port of dspic33ep

Hi,
   This is Rabi. I am working on dspic33ep controller. I want to interface a parallel flash memory with pmp port of my controller.
I am new to this pmp and flash interface. It would be helpful If you can share some samples or related reference files. I installed pheripheral library for development of it. but I am confused where to start. If I have a sample code. It will be helpful.
You can shre me the code to thayarabi@gmail.com  .
Thank you.
#1
RISC
Super Member
  • Total Posts : 5778
  • Reward points : 0
  • Status: offline
RE: parallel flash driver interfaceable with pmp port of dspic33ep 2020/06/24 09:32:46 (permalink)
5 (1)
Hi,
This appnote should be quite helpful to get started even if it was related to the previous dsPIC33 generation :
http://ww1.microchip.com/downloads/en/appnotes/01210a.pdf
Regards
 

For support make sure to check first here : http://microchipdeveloper.com
There are hundreds of PIC, AVR, SAM...which one do YOU use ?
#2
Jump to:
© 2020 APG vNext Commercial Version 4.5