• AVR Freaks

BM64 for transmitter receiver data using PIC32MX470

Author
BENAKKA
New Member
  • Total Posts : 1
  • Reward points : 0
  • Joined: 2020/06/10 00:48:46
  • Location: 0
  • Status: offline
2020/06/22 06:28:36 (permalink)
0

BM64 for transmitter receiver data using PIC32MX470

Hello, 
It's my first post, 
 
I use the PIC32MX470 development card, the aim of the project is to recover the data from the temperature, pressure and humidity sensor by a microcontroller, and transfer it to an Android application using Bluetooth communication.
My question is the following :
Can I use the BM64 Bluetooth 4.2 Stereo audio module for this application or not?

Thanks
#1

0 Replies Related Threads

    Jump to:
    © 2020 APG vNext Commercial Version 4.5