• AVR Freaks

Hot!Harmony v3 Legato: How to change text of labelWidget during run time

Author
marelcom
Starting Member
  • Total Posts : 38
  • Reward points : 0
  • Joined: 2018/01/17 03:18:47
  • Location: 0
  • Status: offline
2020/06/19 07:52:52 (permalink)
0

Harmony v3 Legato: How to change text of labelWidget during run time

Hi

How can I change the text of a legato labelWidget during runtime?
- MPLABX: v5.40
- Harmony: v3
- Grafics Labrary: legato
- XC32: v2.20

Thanks and regards
Markus
#1

2 Replies Related Threads

    MHGC
    Super Member
    • Total Posts : 247
    • Reward points : 0
    • Status: offline
    Re: Harmony v3 Legato: How to change text of labelWidget during run time 2020/06/19 10:32:34 (permalink)
    0
    Hi,
     
    There are two demo applications you may want to reference:
    1) legato_flash
    2) legato_benchmark (gfx_apps repo)
     
    Both of these demo applications have label widgets that are updated within the application code.
    #2
    marelcom
    Starting Member
    • Total Posts : 38
    • Reward points : 0
    • Joined: 2018/01/17 03:18:47
    • Location: 0
    • Status: offline
    Re: Harmony v3 Legato: How to change text of labelWidget during run time 2020/06/22 07:36:42 (permalink)
    0
    Thanks for your help.
    It is working
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5