• AVR Freaks

Hot!MCP2221A: How to change power request

Author
matherp
Starting Member
  • Total Posts : 30
  • Reward points : 0
  • Joined: 2015/02/01 09:01:04
  • Location: 0
  • Status: offline
2020/06/19 06:54:47 (permalink)
0

MCP2221A: How to change power request

The MCP2221A request 100mA from the host and this is controlled through one of its flash registers. I can't find how to change this. Is there some sort of application I can use to connect to it as a HID device to give me access? Any other approach?
Can't see anything on google or the datasheet
 
Thanks
#1

2 Replies Related Threads

    RISC
    Super Member
    • Total Posts : 5776
    • Reward points : 0
    • Status: offline
    Re: MCP2221A: How to change power request 2020/06/19 08:54:44 (permalink)
    4 (1)
    Hi,
    Why do you want to change the 100mA value ?
    There is in fact an HID application but I'm not sure you' ll be able to change this : 
    under the Documents tab you'll find several applications : https://www.microchip.com/wwwproducts/en/MCP2221A
    Regards
    #2
    rjc101
    Super Member
    • Total Posts : 133
    • Reward points : 0
    • Joined: 2016/07/08 14:56:34
    • Location: 0
    • Status: offline
    Re: MCP2221A: How to change power request 2020/06/19 09:34:34 (permalink)
    5 (1)
    You can set the power requested up to 500ma.
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5