• AVR Freaks

Hot!SSH for the PIC32MZ

Author
paul_o
New Member
  • Total Posts : 16
  • Reward points : 0
  • Joined: 2017/11/29 09:15:58
  • Location: 0
  • Status: offline
2020/06/18 08:30:55 (permalink)
4 (1)

SSH for the PIC32MZ

Does anyone know if there's an example app for the PIC32 which includes wolfSSH? In the Harmony v3 download there are examples for wolfSSL client and server, but none for SSH.
 
Thanks in advance.
#1

4 Replies Related Threads

    friesen
    Super Member
    • Total Posts : 2139
    • Reward points : 0
    • Joined: 2008/05/08 05:23:35
    • Location: Indiana, USA
    • Status: offline
    Re: SSH for the PIC32MZ 2020/06/19 12:11:41 (permalink)
    0
    I think you'll have to figure out how to use wolfSSH, or do some other large port job.
     
    If its just a putty console you need, you can do a raw tcp socket easily enough.
     
    Another option: take a library like bearSSL and make a MIT embedded SSH client / server.

    Erik Friesen
    #2
    RISC
    Super Member
    • Total Posts : 5732
    • Reward points : 0
    • Status: online
    Re: SSH for the PIC32MZ 2020/06/19 15:26:02 (permalink)
    0
    Hi,
    If you're ready for some work... : https://www.libssh.org
    Regards
     
    #3
    friesen
    Super Member
    • Total Posts : 2139
    • Reward points : 0
    • Joined: 2008/05/08 05:23:35
    • Location: Indiana, USA
    • Status: offline
    Re: SSH for the PIC32MZ 2020/06/19 16:33:54 (permalink)
    0
    I think it links to openssl, which you probably won't fit on 2MB flash.

    Erik Friesen
    #4
    paul_o
    New Member
    • Total Posts : 16
    • Reward points : 0
    • Joined: 2017/11/29 09:15:58
    • Location: 0
    • Status: offline
    Re: SSH for the PIC32MZ 2020/06/22 01:26:32 (permalink)
    0
    Thanks for the replies. It looks like I'll be persevering with wolfSSH for the time being. I had hoped I could modify a working example to fit my needs rather than building from scratch.
    #5
    Jump to:
    © 2020 APG vNext Commercial Version 4.5