• AVR Freaks

Hot!What does the reset pin actually do on the RN2483?

Author
parkerpics
New Member
  • Total Posts : 2
  • Reward points : 0
  • Joined: 2020/06/09 01:29:54
  • Location: 0
  • Status: offline
2020/06/17 23:37:09 (permalink)
0

What does the reset pin actually do on the RN2483?

Hey,
 
Is the hardware reset pin on the Rn2483 the equivalent of the sys reset command, where the internal configuration is loaded upon reset? 
 
If i need to reset the internal configuration the mac reset command is necessary.
 
So the hardware reset just resets the device whenever we deem necessary, for example to avoid it from getting stuck somehow once in a while. Is my understanding correct?
 
thanks
post edited by parkerpics - 2020/06/18 23:33:28
#1

0 Replies Related Threads

    Jump to:
    © 2020 APG vNext Commercial Version 4.5