• AVR Freaks

Hot!MPLAB X 5.40 / PIC16F15344 - EUSART output to window/file is missing

Author
Ivan Cenov
Super Member
  • Total Posts : 294
  • Reward points : 0
  • Joined: 2003/11/07 12:36:51
  • Location: Bulgaria
  • Status: offline
2020/06/16 04:59:13 (permalink)
5 (1)

MPLAB X 5.40 / PIC16F15344 - EUSART output to window/file is missing

Hi, I am writing to EUSART1 of PIC16F15344 (TX1REG) and want to see the output in the output window of the simulator. However there is no option to activate this function in the project configuration (see the picture below). No support of that function in the simulator for PIC16F15344 yet? Par example it is present for PIC16F18346.
 
Also, what do mean "SIMISA" and "SIMP" columns in Device support list (file:///C:/Program%20Files%20(x86)/Microchip/MPLABX/v5.40/docs/Device%20Support.htm)?

Regards,
Ivan


#1

2 Replies Related Threads

    GeorgePauley
    Moderator
    • Total Posts : 1268
    • Reward points : 0
    • Joined: 2009/12/01 13:59:30
    • Location: Chandler AZ
    • Status: offline
    Re: MPLAB X 5.40 / PIC16F15344 - EUSART output to window/file is missing 2020/06/16 13:30:09 (permalink)
    +1 (1)
    This problem is known, and fixed in 5.45.
     
    ISA = Instruction Set A(something or other)
    P = Peripheral
     
    I have no idea who fills this table or how they decide simulator has ISA or peripheral support.  (And I'm the simulator team lead.)
    #2
    ric
    Super Member
    • Total Posts : 28365
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: online
    Re: MPLAB X 5.40 / PIC16F15344 - EUSART output to window/file is missing 2020/06/16 13:32:13 (permalink)
    0
    Does P perhaps indicate if some peripherals are not implemented?
     

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5