• AVR Freaks

Hot!BM70, COMMAND SET PROTOCOL, Other Responses as explained in the manual

Author
McLion
New Member
  • Total Posts : 4
  • Reward points : 0
  • Joined: 2003/11/07 12:44:23
  • Status: offline
2020/06/08 06:12:25 (permalink)
4 (1)

BM70, COMMAND SET PROTOCOL, Other Responses as explained in the manual

Hi,
We use a BM70 with the newest Firmware (v1.11).
If I send a protocol (write the advertising data) (AA 00 06 11 03 06 08 D7) during the module is in configure mode 
I get this answer (Complete Event) (AA 00 03 80 11 00 6C). The advertising data succesfully changed.
 
In the newest manual, the answer of to the write advertising data should be (AA 00 01 80 1 Byte Answer 1 Byte Checksum)
In real there is one more byte (the op code is additionally in the protocoll).
According the manual (DS50002542A page 171) the length is 1, but in this example the length should be 2 (80 and the answer byte). 
 
Could it be that this manual on the microchips website isnt't the newest one? This is untypical for manuals from microchip.
 
Cheers 
 
 
#1

0 Replies Related Threads

    Jump to:
    © 2020 APG vNext Commercial Version 4.5