• AVR Freaks

Hot!mplab data visualizer install fail

Author
robertz
New Member
  • Total Posts : 10
  • Reward points : 0
  • Joined: 2020/05/25 23:31:04
  • Location: 0
  • Status: offline
2020/06/05 00:50:10 (permalink)
0

mplab data visualizer install fail

hi, all,
  i plan to install mplab data visualizer plug-in in MPLAB ide v5.25; but it tip need to install MatchToolCommPort v1.1, current is v1.0, but i can not find where is version 1.1 of MatchToolCommPoart plug-in to install or update;
who know how to do it?
#1

3 Replies Related Threads

    stevereinert
    Super Member
    • Total Posts : 150
    • Reward points : 0
    • Joined: 2010/05/12 09:20:48
    • Location: Chandler, AZ
    • Status: offline
    Re: mplab data visualizer install fail 2020/06/17 15:27:28 (permalink)
    0
    Hello,
     
    The MPLAB Data Visualizer plugin v1.0 and above require MPLAB X IDE 5.30 and above.  It's not compatible with v5.25.  The error message you're seeing for MatchToolCommPort plugin v1.1 not found is because this is only available in 5.30 and up. 
     
    There is a standalone installer version of MPLAB Data Visualizer if you need to stay on 5.25 and would still like to use it.  You can find that here: https://gallery.microchip.com/packages?q=Tags%3A%22DataVisualizer_Standalone_MPLAB%22
     
    #2
    robertz
    New Member
    • Total Posts : 10
    • Reward points : 0
    • Joined: 2020/05/25 23:31:04
    • Location: 0
    • Status: offline
    Re: mplab data visualizer install fail 2020/06/17 17:31:55 (permalink)
    0
    i install a standalone version of data visualizer, but after connect serial port, can not add ds file on data streamer item.
    i also check the 'autodetect protocols' item.
    #3
    stevereinert
    Super Member
    • Total Posts : 150
    • Reward points : 0
    • Joined: 2010/05/12 09:20:48
    • Location: Chandler, AZ
    • Status: offline
    Re: mplab data visualizer install fail 2020/06/18 10:05:34 (permalink)
    0
    Hi,
    The autodetect protocols is not supported yet in MPLAB Data Visualizer.  That support is planned for a future release.  Regarding loading a DS file, there's an Import button available on the Variable Streamers tab. This works with .ds files.  See here for the documentation on that:
    https://onlinedocs.microchip.com/pr/GUID-4FF3C687-0C30-4D21-82D0-5AE401E8BE9D-en-US-2/index.html?GUID-BC9657C4-6682-452F-9799-1AA04F2D99AD
     
    #4
    Jump to:
    © 2020 APG vNext Commercial Version 4.5