• AVR Freaks

WINC1500 connection fails

Author
128 bits
New Member
  • Total Posts : 3
  • Reward points : 0
  • Joined: 2020/06/01 02:19:05
  • Location: 0
  • Status: offline
2020/06/04 02:51:50 (permalink)
0

WINC1500 connection fails

Hi,
We have a custom board with an Xmega256, where we have made an adoption of the asf library for the Winc1500 (since the Xmega isn’t supported).
Scanning and finding our network works fine. It initiates the connection, but it never succeeds and says that the state changed to disconnected, which goes on forever.
I am stuck with this problem, and hope that someone could give me some ideas for how to proceed. I am not sure if we did something wrong when porting to Xmega, or if it could be a configuration of the Winc. Any small clue or idea is highly appreciated!
 
This is the output:
(APP)(INFO)Chip ID 1503a0
(APP)(INFO)DriverVerInfo: 0x13301361
(APP)(INFO)Firmware ver : 19.6.1 Svnrev 16761
(APP)(INFO)Firmware Build May 23 2018 Time 14:39:16
(APP)(INFO)Firmware Min driver ver : 19.3.0
(APP)(INFO)Driver ver: 19.6.1
(APP)(INFO)Driver built at Jun 1 2020 15:39:40
Wifi connect: 0
wifi_cb: M2M_WIFI_RESP_CON_STATE_CHANGED: DISCONNECTED (error code: 3)
wifi_cb: M2M_WIFI_RESP_CON_STATE_CHANGED: DISCONNECTED (error code: 3)
wifi_cb: M2M_WIFI_RESP_CON_STATE_CHANGED: DISCONNECTED (error code: 1)
wifi_cb: M2M_WIFI_RESP_CON_STATE_CHANGED: DISCONNECTED (error code: 3)
:

 
And this is the code where the disconnect message is generated:
case M2M_WIFI_RESP_CON_STATE_CHANGED:
{
tstrM2mWifiStateChanged *pstrWifiState = (tstrM2mWifiStateChanged *)pvMsg;
 if (pstrWifiState->u8CurrState == M2M_WIFI_CONNECTED) {
   printf("wifi_cb: M2M_WIFI_RESP_CON_STATE_CHANGED: CONNECTED\r\n");
   m2m_wifi_request_dhcp_client();
 } else if (pstrWifiState->u8CurrState == M2M_WIFI_DISCONNECTED) {
  printf("wifi_cb: M2M_WIFI_RESP_CON_STATE_CHANGED: DISCONNECTED (error code: %u)\r\n", pstrWifiState->u8ErrCode);
  wifi_connected = 0;
  m2m_wifi_connect((char *)MAIN_WLAN_SSID, sizeof(MAIN_WLAN_SSID), MAIN_WLAN_AUTH, (char *)MAIN_WLAN_PSK, M2M_WIFI_CH_ALL);
 }

 break;

#1

0 Replies Related Threads

    Jump to:
    © 2020 APG vNext Commercial Version 4.5