• AVR Freaks

Hot!PIC32 Simulation in any program (Proteus, Multisim etc.)

Author
captain25
New Member
  • Total Posts : 12
  • Reward points : 0
  • Joined: 2020/04/12 06:14:10
  • Location: 0
  • Status: offline
2020/06/03 11:44:35 (permalink)
2 (1)

PIC32 Simulation in any program (Proteus, Multisim etc.)

I want to make a project with PIC32 MZ. But I couldn't find this microcontroller in simulation programs. I noticed that there was no PIC32 model, not just that model.
Is it possible to add an external library for those who want to work on this subject? Or if there is such a version, can the link be shared?
 
Best regards
#1

3 Replies Related Threads

    ric
    Super Member
    • Total Posts : 28009
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: offline
    Re: PIC32 Simulation in any program (Proteus, Multisim etc.) 2020/06/03 16:42:31 (permalink)
    5 (1)
    Why not ask the authors of those programs? They are not Microchip products.
     

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #2
    captain25
    New Member
    • Total Posts : 12
    • Reward points : 0
    • Joined: 2020/04/12 06:14:10
    • Location: 0
    • Status: offline
    Re: PIC32 Simulation in any program (Proteus, Multisim etc.) 2020/06/04 01:23:23 (permalink)
    0
    The programs are not Microchip products, of course. But what I want to simulate is the Microchip product.
     
    I asked this question with the assumption that there is someone here who has noticed this problem before and found a solution.
    post edited by captain25 - 2020/06/04 12:31:10
    #3
    captain25
    New Member
    • Total Posts : 12
    • Reward points : 0
    • Joined: 2020/04/12 06:14:10
    • Location: 0
    • Status: offline
    Re: PIC32 Simulation in any program (Proteus, Multisim etc.) 2020/06/04 12:54:15 (permalink)
    0
    Simulation is a very important stage in the project. I would be glad if someone who knows can answer as soon as possible.
    #4
    Jump to:
    © 2020 APG vNext Commercial Version 4.5