• AVR Freaks

Hot!dsPIC33CK Curiosity, compiler does'nt work [solved]

Author
hansp
Starting Member
  • Total Posts : 32
  • Reward points : 0
  • Joined: 2020/04/03 10:40:27
  • Location: Austria
  • Status: offline
2020/05/30 09:05:27 (permalink)
5 (1)

dsPIC33CK Curiosity, compiler does'nt work [solved]

Hi,

now I'm trying to get the board up and running. I installed the pack dsPIC33CK-MP_DFP. It is strange that is displayed in the customize window "ds_PIC33_Harmony". The MCC works as usual. If I now click on the" hammer symbol" I get the following error message:
"nbproject/Makefile-dsPIC33_Harmony.mk:131: *** missing 'endif'.  Stop."
What is wrong?
BR
Peter
 
post edited by hansp - 2020/05/30 11:31:40
#1

3 Replies Related Threads

    hansp
    Starting Member
    • Total Posts : 32
    • Reward points : 0
    • Joined: 2020/04/03 10:40:27
    • Location: Austria
    • Status: offline
    Re: dsPIC33CK Curiosity, compiler does'nt work 2020/05/30 11:31:23 (permalink)
    0
    Sorry, it was my mistake, I generated the project as "harmony Project".

    Now I created it as a stand allone project and it works.
     
    #2
    TS9
    Super Member
    • Total Posts : 908
    • Reward points : 0
    • Joined: 2010/05/07 10:52:22
    • Status: offline
    Re: dsPIC33CK Curiosity, compiler does'nt work 2020/05/30 11:39:42 (permalink)
    0
    Great !!!
    #3
    hansp
    Starting Member
    • Total Posts : 32
    • Reward points : 0
    • Joined: 2020/04/03 10:40:27
    • Location: Austria
    • Status: offline
    Re: dsPIC33CK Curiosity, compiler does'nt work 2020/06/02 08:36:45 (permalink)
    0
    No, not great, I'am ashamed because such a simple mistake.
    #4
    Jump to:
    © 2020 APG vNext Commercial Version 4.5