• AVR Freaks

Hot!dsPIC33CK256MP508 dual core?

Author
hansp
Starting Member
  • Total Posts : 32
  • Reward points : 0
  • Joined: 2020/04/03 10:40:27
  • Location: Austria
  • Status: offline
2020/05/29 23:58:41 (permalink)
2 (1)

dsPIC33CK256MP508 dual core?

Hello friends,

I have now installed a curiosity board with the dsPIC33CK256MP508. But I'm a little confused. In MCC adc1 configuration you have to set core0 / core1 / shared for the channels but there is no slave core in the device recources. What now?
 
BR
Peter
#1

2 Replies Related Threads

    du00000001
    Just Some Member
    • Total Posts : 3942
    • Reward points : 0
    • Joined: 2016/05/03 13:52:42
    • Location: Germany
    • Status: offline
    Re: dsPIC33CK256MP508 dual core? 2020/05/30 03:07:41 (permalink)
    5 (1)
    "slave core" like in "slave microcontroller core"?
    Could it be you've mistaken the CK family (single microcontroller core) for the CH family (dual core) ?
     
    ("core0/1/shared" is just about ADC converter "cores".)

    PEBKAC / EBKAC / POBCAK / PICNIC (eventually see en.wikipedia.org)
    #2
    hansp
    Starting Member
    • Total Posts : 32
    • Reward points : 0
    • Joined: 2020/04/03 10:40:27
    • Location: Austria
    • Status: offline
    Re: dsPIC33CK256MP508 dual core? 2020/05/30 08:58:34 (permalink)
    0
    Thank you,
    now I understand.
     
    BR Peter
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5