• AVR Freaks

Hot!CANT USE STOPWATCH WITH BREAK POINTS USING SNAP.

Author
zoopi
New Member
  • Total Posts : 21
  • Reward points : 0
  • Joined: 2020/03/28 04:39:38
  • Location: 0
  • Status: offline
2020/05/29 21:51:54 (permalink)
5 (1)

CANT USE STOPWATCH WITH BREAK POINTS USING SNAP.

Hi all, 
Am trying to calculate the execution time of part of my code. But when I open stopwatch and try to set the start and stop positions according to the break points, its showing this function is not available with your tool. Same scenario also with mpsim.
if its not possible then how to calculate timing of part of my code.

Attached Image(s)

#1

4 Replies Related Threads

    DevMod1
    Administrator
    • Total Posts : 532
    • Reward points : 0
    • Joined: 2009/02/10 09:34:30
    • Location: 0
    • Status: offline
    Re: CANT USE STOPWATCH WITH BREAK POINTS USING SNAP. 2020/06/01 10:11:44 (permalink)
    0
    What device are you using??

    _____________________________

    Please read the forum posting guidelines. Do not double post, please help keep these forums professional and comments respectful.
    Please notify the moderators of problems/spam/trolls.
    #2
    zoopi
    New Member
    • Total Posts : 21
    • Reward points : 0
    • Joined: 2020/03/28 04:39:38
    • Location: 0
    • Status: offline
    Re: CANT USE STOPWATCH WITH BREAK POINTS USING SNAP. 2020/06/05 23:03:15 (permalink)
    0
    DevMod1
    What device are you using??


    PIC18F47Q43
    CLOCK 16000000
    #3
    MHS
    Super Member
    • Total Posts : 367
    • Reward points : 0
    • Joined: 2010/04/23 10:05:39
    • Location: 0
    • Status: offline
    Re: CANT USE STOPWATCH WITH BREAK POINTS USING SNAP. 2020/06/08 17:25:50 (permalink)
    0
    Per this document http://ww1.microchip.com/downloads/en/DeviceDoc/HWToolDebugFeatures_v5.40.pdf this device doesn't support the Stopwatch feature.
     
    You can try the simulator.
    #4
    ric
    Super Member
    • Total Posts : 28324
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: online
    Re: CANT USE STOPWATCH WITH BREAK POINTS USING SNAP. 2020/06/08 17:34:00 (permalink)
    0
    Or modify your code to toggle a pin high at the start, and low at the end, and use a storage scope to measure the width of the pulse.
     

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #5
    Jump to:
    © 2020 APG vNext Commercial Version 4.5