MPLABX Project Properties Dialogue Window - Unable to read settings
I'm using MPLAB X IDE v5.40 (was same in 5.35) with Linux Ubuntu 19.10.
I've been getting XC8 complier warning messages (373 implicit signed to unsigned conversion) which i'm not worried about, so I tried to change the compiler warning level from -3 to -2, which is located in the Project Properties window.
Unfortunately the data in this window for (Simulator, XC8 Global Options, XC8 Complier & XC8 Linker) does not display correctly (seems the font is too high for the boxes) and it is very difficult to read and see what changes you are making.
The screenshot shows the issue - look at the "Warning level" value - currently -3.
I've tried changing my display resolution but the problem remains.
Is this unique to Linux/Ubuntu or does it apply to other platforms too?
Attachment(s)
Attachments are not available: Download requirements not met