• AVR Freaks

Hot!Move project from PIC32MZ DAH to DAR chip- harmony/compiler problem

Author
kuku
Senior Member
  • Total Posts : 143
  • Reward points : 0
  • Joined: 2012/03/03 08:05:54
  • Location: 0
  • Status: offline
2020/05/23 03:45:19 (permalink)
0

Move project from PIC32MZ DAH to DAR chip- harmony/compiler problem

For DAH I use 2.15 compiler. DAR need younger version so I install 2.41. Harmony is still 2.06.
When I try to compile my project I see only error, also from harmony configurator lost pin configurator (or I cannot find it), clock settings are destroyed, etc.
 
Is any tip or DAR work only with Harmony v3?
post edited by kuku - 2020/05/23 06:20:08
#1

2 Replies Related Threads

    arpananand
    Super Member
    • Total Posts : 498
    • Reward points : 0
    • Joined: 2009/11/18 04:35:42
    • Location: 0
    • Status: offline
    Re: Move project from PIC32MZ DAH to DAR chip- harmony/compiler problem 2020/05/26 08:38:14 (permalink)
    5 (1)
    Harmony 2 as it is doesn't support  newer version of DA series of silicon. either you need to switch to Harmony 3 or you need to do minor tweaks in Harmony 2 to make it work.
    #2
    Stefiff
    Senior Member
    • Total Posts : 99
    • Reward points : 0
    • Joined: 2012/07/15 15:26:29
    • Location: 0
    • Status: offline
    Re: Move project from PIC32MZ DAH to DAR chip- harmony/compiler problem 2020/05/26 13:10:36 (permalink)
    0
    I use DAS with H3. Working properly. In H2 processor does not exist at all.
    Unfortunately there are some “weird things” with some modules that are not described in the errata file. The software needs to be adjusted in some places according to how the module works. If you use a Harmony, it's not your concern.
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5