• AVR Freaks

Hot!USB2514B

Author
B.Kaavya
New Member
  • Total Posts : 5
  • Reward points : 0
  • Joined: 2019/09/02 23:51:17
  • Location: 0
  • Status: offline
2020/05/12 04:00:17 (permalink)
0

USB2514B

Hi Team,
Wishing you a good day.
Can you please conform that the following Microchip chip-set are compatible with Android 9.0 and Linux OS .
Also please share if any software drivers available of the chip-sets or not.
USB HUB : USB5744/2G ,USB2514B .
USB to Ethernet bridge: LAN7800/VSX , LAN7500.
 
Thanks and Regards,
Kaavya.
post edited by B.Kaavya - 2020/05/14 11:57:02
#1
roundrocktom
Super Member
  • Total Posts : 1047
  • Reward points : 0
  • Joined: 2012/09/07 08:19:09
  • Location: Texas
  • Status: offline
Re: USB2514B 2020/05/15 07:05:42 (permalink)
3.67 (3)
The forum is a peer to peer group (not necessarily monitored by Microchip).
Official inquiries should go into the Microchip Support Page.
https://microchipsupport.force.com/s/article/How-to-submit-a-case
 
Having said that. Those parts are common to USB Hubs and the USB to Ethernet are well supported. Drivers are native to Andriod and Linux.
 
I have found Microchip's "Design Check" is super helpful on USB and Ethernet designs. A second set of eyes to help catch issues. Look for "schematic checklist" under that USB to Ethernet devices.
https://www.microchip.com/design-check-services
 
 
 
#2
Jump to:
© 2020 APG vNext Commercial Version 4.5