• AVR Freaks

Hot!Problem finding compatibility of SAM3A8C with Arduino IDE

Author
rajkumar kaliaperumal
New Member
  • Total Posts : 3
  • Reward points : 0
  • Joined: 2020/05/08 04:29:01
  • Location: 0
  • Status: offline
2020/05/10 22:04:53 (permalink)
0

Problem finding compatibility of SAM3A8C with Arduino IDE

Hi ,
     I have a system which uses SAM3X8E as my base board. Since i don't require a large number of PIO's and want to reduce the board size ,i would like to replace SAM3X8E LQFP144 PIN IC with SAM3A8C LQFP100 PIN IC.The problem is i couldn't get much information on the internet regarding SAM3A8C whether it is compatible with Arduino IDE or not.
 
     I provide what little information i have,
         -  SAM3X8E and SAM3A8C both has same datasheet, only difference is the number of pins.
         -  Since the difference between the boards(mostly) is number of pins i hope pin Configurations will be one of the issues.
         -  I found a file with register and other configurations of SAM3A8C in arduino IDE folder and with that i guess the SAM3A8C might be compatible with arduino IDE.

         configuration file location (in windows)- C:\Users\SYSTEMNAME\AppData\Local\Arduino15\packages\arduino\hardware\sam\1.6.12\system\CMSIS\Device\ATMEL\sam3xa\include\SAM3A8C.h

questions:
      - Whether the IDE will be able to identify the SAM3A8C? (Since there is no arduino Board with SAM3A8C)
      - If it is possible then, is there any other issues to program it??
      - If there is any other IDE suggestions i would like to hear that as well.
#1

0 Replies Related Threads

    Jump to:
    © 2020 APG vNext Commercial Version 4.5