• AVR Freaks

AnsweredHot!Compilation error when accessing DMA data space with pointer

Page: < 12 Showing page 2 of 2
Author
dspic
Starting Member
  • Total Posts : 36
  • Reward points : 0
  • Joined: 2008/09/08 18:10:10
  • Location: 0
  • Status: offline
Re: about DMA data access 2020/05/09 23:56:47 (permalink)
4.5 (2)
The problem I have encountered solved, I hope this post has a reference for other engineers. Thanks to JPortici, ric, Jtemples for their warm guidance and help, thank you very much!
#21
JPortici
Super Member
  • Total Posts : 1105
  • Reward points : 0
  • Joined: 2012/11/17 06:27:45
  • Location: Grappaland
  • Status: offline
Re: about DMA data access 2020/05/11 21:56:09 (permalink)
0
so i see the question. Please read the compiler manual and the 16bit language tool libraries, also in the compiler document folder.
 
There is more than one memcpy definition. one with both argument in near data space, one with both argument in eds space. You can't use the normal memcpy as it assumes both argument are NOT in eds (for which you have to set up the device for access)
#22
Page: < 12 Showing page 2 of 2
Jump to:
© 2020 APG vNext Commercial Version 4.5