• AVR Freaks

Hot!which devboards have the PKOB4?

Author
JPortici
Super Member
  • Total Posts : 1114
  • Reward points : 0
  • Joined: 2012/11/17 06:27:45
  • Location: Grappaland
  • Status: offline
2020/05/05 08:09:43 (permalink)
0

which devboards have the PKOB4?

Is there a list somewhere of the boards that are now coming with the PKOB4 (which is a pickit4 "on board")?
 
There are two obvious advantages.
the PKOB3 has always been well.. awful. (other words come to mind though), supposedly the PKOB4 will have more or less the same hardware and firmware as the PK4, with all the improvements in programming and debugging speed.
Also, the PKOB4 enumerates a companion virtual com port too that may come in handy.
 
Yes, one can (almost) always connect an external debugger but i believe one cable instead of three is usually better. (why three? 1)power 2)debugger 3)com port))
 
Known Devboards with PKOB4
DM164136 - Curiosity High Pin Count (HPC) Development Board
DM164137 - Curiosity Development Board (recent version)
DM320209 - Curiosity PIC32MZ EF 2.0 Development Board
DM330030 - dsPIC33CK Curiosity Development Board
post edited by JPortici - 2020/05/28 06:02:44
#1

10 Replies Related Threads

    katela
    Super Member
    • Total Posts : 1833
    • Reward points : 0
    • Joined: 2013/06/11 05:25:18
    • Location: South Africa
    • Status: offline
    Re: which devboards have the PKOB4? 2020/05/05 09:58:24 (permalink)

    Free online Microcontroller Tutorials and Projects for Hobbyists and students. From beginners to advanced. Website: www.studentcompanion.co.za
    YouTube Tutorials: https://www.youtube.com/StudentCompanionSA
    #2
    JPortici
    Super Member
    • Total Posts : 1114
    • Reward points : 0
    • Joined: 2012/11/17 06:27:45
    • Location: Grappaland
    • Status: offline
    Re: which devboards have the PKOB4? 2020/05/05 13:10:49 (permalink)
    0
    Yes, it seems that the new curiosity boards come with the PKOB4 (i was pondering on buying a new 16 or 32bit devboard to experiment with uC/OS now that os and related tools and books have become free)
    #3
    NKurzman
    A Guy on the Net
    • Total Posts : 18859
    • Reward points : 0
    • Joined: 2008/01/16 19:33:48
    • Location: 0
    • Status: online
    Re: which devboards have the PKOB4? 2020/05/05 14:05:31 (permalink)
    0
    uC/OS as in Micrium?  Which Version?
     
    #4
    MCHP_Admin
    MCHP_Admin
    • Total Posts : 26
    • Reward points : 0
    • Status: offline
    Re: which devboards have the PKOB4? 2020/05/05 14:30:51 (permalink)
    0
    The Curiosity Low Pin count board supporting 20 pins and below also has the PKOB4
    #5
    JPortici
    Super Member
    • Total Posts : 1114
    • Reward points : 0
    • Joined: 2012/11/17 06:27:45
    • Location: Grappaland
    • Status: offline
    Re: which devboards have the PKOB4? 2020/05/05 14:43:06 (permalink)
    0
    NKurzman
    uC/OS as in Micrium?  Which Version?



    2,3, whichever (but i'm reading the book on 3). i have to do manual work anyway as the few examples from microchip are from 6 years ago. no RTOS support for PIC32 in harmony 3 either :(
    post edited by JPortici - 2020/05/05 14:44:44
    #6
    NKurzman
    A Guy on the Net
    • Total Posts : 18859
    • Reward points : 0
    • Joined: 2008/01/16 19:33:48
    • Location: 0
    • Status: online
    Re: which devboards have the PKOB4? 2020/05/05 16:36:02 (permalink)
    0
    I do not think uC/OS-II or uC/OS-III is free for Commercial Use.  Harmony V1,2  supported  uC/OS ( Not sure about 3), and FreeRTOS.  I heard that Harmony 3 Defaults to FreeRTOS.  The Default for Harmony 1 and 2 was No RTOS.
    #7
    JPortici
    Super Member
    • Total Posts : 1114
    • Reward points : 0
    • Joined: 2012/11/17 06:27:45
    • Location: Grappaland
    • Status: offline
    Re: which devboards have the PKOB4? 2020/05/05 22:53:17 (permalink)
    0
    so you didn't hear the news :) https://www.micrium.com/buy/licensing/
    it was in the latest Embedded Muse
     
    In any case, whichever RTOS support harmony 3 may support, not for PIC32 is supported, yet. (there are two repositories, one for CMSIS-FreeRTOS so ATSAM only and one for uC/OS-III which is currently only ATSAM)
    #8
    RISC
    Super Member
    • Total Posts : 5776
    • Reward points : 0
    • Status: offline
    Re: which devboards have the PKOB4? 2020/05/26 08:23:48 (permalink)
    4.5 (2)
    Known Devboards with PKOB4
    DM164136 - Curiosity High Pin Count (HPC) Development Board (recent version)
    DM164137 - Curiosity Low Pin Count (LPC) Development Board (recent version)
    DM320209 - Curiosity PIC32MZ EF 2.0 Development Board
    DM330030 - dsPIC33CK Curiosity Development Board
     
    post edited by RISC - 2020/05/28 14:10:56
    #9
    Howard Long
    Super Member
    • Total Posts : 796
    • Reward points : 0
    • Joined: 2005/04/04 08:50:32
    • Status: offline
    Re: which devboards have the PKOB4? 2020/05/28 04:13:21 (permalink)
    0
    RISC
    DM164136 - Curiosity High Pin Count (HPC) Development Board (recent version)
    DM164137 - Curiosity Development Board (recent version)



    I guess there's not way of knowing when you order which you're going to get? Coincidentally I ordered a backup HPC board a week or so ago as the one I currently have has been seeing a lot of use. After reading this thread I note that the new one does indeed have the PKOB4.
     
    All of the Nano boards I have use a "PKOB Nano" debugger, seemingly from the Xplained series as far as a cursory view tells me, but ISTBC. Perhaps that's still PKOB4, but the behavior under the hood seems a little different as far as I can tell.
     
    #10
    judd
    Starting Member
    • Total Posts : 51
    • Reward points : 0
    • Joined: 2019/04/15 22:30:22
    • Location: 0
    • Status: offline
    Re: which devboards have the PKOB4? 2020/05/28 12:50:35 (permalink)
    0
    Howard Long
    Perhaps that's still PKOB4, but the behavior under the hood seems a little different as far as I can tell.

    Indeed the PKoB Nano is a "nEDBG" under the hood; more closely related to the EDBG on Xplained series than it is the PKoB4.


    #11
    Jump to:
    © 2020 APG vNext Commercial Version 4.5