• AVR Freaks

Hot!WINC1500 porting and DMA

Author
matjaz
New Member
  • Total Posts : 1
  • Reward points : 0
  • Joined: 2020/04/26 04:01:07
  • Location: 0
  • Status: offline
2020/04/27 03:27:01 (permalink)
0

WINC1500 porting and DMA

Hi
I am trying to make WINC1500 WiFi module work with ST microcontroller. As sugested in Microchip's document I implemented all the required stub functions, created 1ms timer and enabled externall interrupt. Now I can succesfuly read ID of chip.
But when I try to connect to my WiFi using first:
m2m_wifi_init();
m2m_wifi_connect();

Module can't get DMA address. What am I doing wrong?
#1

0 Replies Related Threads

    Jump to:
    © 2020 APG vNext Commercial Version 4.5