• AVR Freaks

Hot!Create screen dynamically and destroy it at the end

Author
epareja
Super Member
  • Total Posts : 380
  • Reward points : 0
  • Joined: 2003/11/07 12:53:08
  • Location: Colombia
  • Status: offline
2020/04/10 15:30:23 (permalink)
0

Create screen dynamically and destroy it at the end

Hello,
 
I'm using Harmony 2.06b and Aria graphic library. I have created screens in the graphics composer that are created at the beginning of the application, but I want to create the screens at runtime when needed.
I know how to create the screens but any advise on how to handle the OnCreate and destroy methods?
 
Thank you
post edited by epareja - 2020/04/13 08:28:40


Ernesto Pareja J
www.dcctrains.netne.net

#1

2 Replies Related Threads

    MHGC
    Super Member
    • Total Posts : 247
    • Reward points : 0
    • Status: offline
    Re: Create screen dynamically and destroy it at the end 2020/04/17 11:08:42 (permalink)
    0
    Hi,

    You will need to add/remove screens to the Aria context using laContext_AddScreen/laContext_RemoveScreen.   
    You may want to look at libaria_init.c.  This is the generated output from Harmony Graphics Composer, it shows how the designed screens are handled.
    #2
    epareja
    Super Member
    • Total Posts : 380
    • Reward points : 0
    • Joined: 2003/11/07 12:53:08
    • Location: Colombia
    • Status: offline
    Re: Create screen dynamically and destroy it at the end 2020/05/18 19:06:08 (permalink)
    0
    Thank you for your answer. That's what I'm doing but I would like to know if there is a configuration to make the libaria_initialize() function to omit the screen creation.
    I'm having to edit manually that function and I have to verify every change in the screen arrangement.
     
    To free the memory I know I have to call laScreen_Destroy(&screen); but I would like to know a good method to destroy the screen when pushed a button on the same screen.
     
    Also, I would like to know if laContext_RemoveScreen free the memory in the heap.
     
    Thank you.
     
    post edited by epareja - 2020/05/18 19:10:44


    Ernesto Pareja J
    www.dcctrains.netne.net

    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5