• AVR Freaks

Hot!Harmony 2 & macOS Catalina

Author
SincPelp
New Member
  • Total Posts : 5
  • Reward points : 0
  • Joined: 2020/03/17 08:55:32
  • Location: 0
  • Status: offline
2020/04/08 11:39:05 (permalink)
0

Harmony 2 & macOS Catalina

Hi.
Does anyone know how I can install Harmony 2 on MacOs Catalina?
Is it possible to migrate a harmony 2 project to harmony 3?
Thank you.
#1

1 Reply Related Threads

    nigelwright7557
    Super Member
    • Total Posts : 422
    • Reward points : 0
    • Joined: 2006/11/06 08:15:51
    • Location: 0
    • Status: online
    Re: Harmony 2 & macOS Catalina 2020/04/08 16:04:00 (permalink)
    0
    I recently converted harmony 2 project to harmony 3.
    I found I had to create a new harmony 3 project then add modules as required to the new project.
    It took a while to get it working right as H3 is a bit different.
     
    Sorry cant help with the mac as I am a Win PC man.
     
    #2
    Jump to:
    © 2020 APG vNext Commercial Version 4.5