• AVR Freaks

Hot!How to store video file in Program memory

Author
malaksal
New Member
  • Total Posts : 4
  • Reward points : 0
  • Joined: 2017/03/14 02:35:03
  • Location: 0
  • Status: offline
2020/04/08 05:13:14 (permalink)
0

How to store video file in Program memory

hello
   I am using Pic32mz2048efh100 with MPLAB x ide and I am trying to send a movie file over UART interface to another micro controller for that i need to store the video file into program memory.
There is no constraints on the length or size of the video i just want to make sure that i can send it.
How can I store the video file into program memory. (how to converted to binary? or is there an another way?)

best regards
 
 
#1

3 Replies Related Threads

    crosland
    Super Member
    • Total Posts : 1936
    • Reward points : 0
    • Joined: 2005/05/10 10:55:05
    • Location: Warks, UK
    • Status: offline
    Re: How to store video file in Program memory 2020/04/08 06:33:27 (permalink)
    0
    malaksal
    How can I store the video file into program memory.

     
    Have you read the FLASH programming section of the datasheet for the device you are using?
     
    malaksal
     (how to converted to binary? or is there an another way?)

     
    If it's not binary, what do you think it is?
     
    Seriously, You seem to be lacking some fundamental knowledge to attempt this task. I would start with something simpler.
     
    Write some simple code to write to the program FLASH. Come back with the issues you encounter when you have actually tried something.
     
     
    #2
    NKurzman
    A Guy on the Net
    • Total Posts : 18655
    • Reward points : 0
    • Joined: 2008/01/16 19:33:48
    • Location: 0
    • Status: online
    Re: How to store video file in Program memory 2020/04/08 07:51:20 (permalink)
    0
    Are you trying to include it in a program?
    Or send it to the micro processor and store it there programmatically?
    #3
    friesen
    Super Member
    • Total Posts : 2123
    • Reward points : 0
    • Joined: 2008/05/08 05:23:35
    • Location: Indiana, USA
    • Status: offline
    Re: How to store video file in Program memory 2020/04/08 11:28:50 (permalink)
    0
    What will there be, about 2 seconds of video capability on the biggest flash part?

    Erik Friesen
    #4
    Jump to:
    © 2020 APG vNext Commercial Version 4.5