• AVR Freaks

Hot!SPI Communication in PIC32MX470F512H with MPU9250

Author
Mustafaa
New Member
  • Total Posts : 4
  • Reward points : 0
  • Joined: 2020/02/19 06:18:41
  • Location: 0
  • Status: offline
2020/04/05 09:25:56 (permalink)
0

SPI Communication in PIC32MX470F512H with MPU9250

Hi everyone, how can i do spi communication between mpu9250 and pic32mx470f512h?
I'm using xc32,harmony v2.06
Thanks.
#1

2 Replies Related Threads

    ric
    Super Member
    • Total Posts : 27629
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: online
    Re: SPI Communication in PIC32MX470F512H with MPU9250 2020/04/05 13:29:11 (permalink)
    0
    Step#1 have you read the datasheets for both devices?
    #2 have you ever used SPI before?
     

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #2
    Mustafaa
    New Member
    • Total Posts : 4
    • Reward points : 0
    • Joined: 2020/02/19 06:18:41
    • Location: 0
    • Status: offline
    Re: SPI Communication in PIC32MX470F512H with MPU9250 2020/04/06 03:45:31 (permalink)
    0
    Hi,
    Yes i read both of them datasheets and no i dont use spi before. 
    Thanks
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5