• AVR Freaks

Hot!Where to define "Enviromental Variables" ?

Author
erikS
New Member
  • Total Posts : 5
  • Reward points : 0
  • Joined: 2009/03/08 10:11:25
  • Location: Germany
  • Status: offline
2020/04/04 05:03:31 (permalink)
0

Where to define "Enviromental Variables" ?

Hello,
I read the XC16 manual. "5.2.2 Environment Variables" says if a variable  from Table 5-1 is defined the compiler will use it. I have no idea how to define this variable. Can anybody give me a example how to define XC16_C_INCLUDE_PATH in MPLAB X? I know I can enter paths in MPLAB X which will end in the -I option but this is not my question. I will lern the other option.
#1

2 Replies Related Threads

    du00000001
    Just Some Member
    • Total Posts : 3665
    • Reward points : 0
    • Joined: 2016/05/03 13:52:42
    • Location: Germany
    • Status: offline
    Re: Where to define "Enviromental Variables" ? 2020/04/04 05:35:39 (permalink)
    0
    Windows?
    These settings are accessible via the System Control Panel. To get there really changed from (Windows) version to version  :(
    This one might help:
    https://support.shotgunsoftware.com/hc/en-us/articles/114094235653-Setting-global-environment-variables-on-Windows?mobile_site=true
    Or g..gl. for "environment variables setting" (without the quotes) and use wharever links seems to be understandable for you.

    PEBKAC / EBKAC / POBCAK / PICNIC (eventually see en.wikipedia.org)
    #2
    erikS
    New Member
    • Total Posts : 5
    • Reward points : 0
    • Joined: 2009/03/08 10:11:25
    • Location: Germany
    • Status: offline
    Re: Where to define "Enviromental Variables" ? 2020/04/04 12:16:10 (permalink)
    0
    Yes, Windows 10. I define the Environment variable XC16_C_INCLUDE_PATH in Control Panel with value C:\tmp and restart Windows and MPLAB X. I place a test Header in C:/tmp but the Compiler will not find the file, so this way seems not working:-(
    post edited by erikS - 2020/04/04 12:17:35

    Attached Image(s)

    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5