• AVR Freaks

Hot!Configuring the LoRa demo code (SAMR34Xplained) to work woth the SAMR35

Author
ianharvey
New Member
  • Total Posts : 9
  • Reward points : 0
  • Joined: 2009/05/14 06:17:47
  • Location: 0
  • Status: offline
2020/04/01 02:36:07 (permalink)
0

Configuring the LoRa demo code (SAMR34Xplained) to work woth the SAMR35

HI,
I am using the demo code for the SAMR34 board as the basis for my design, but I am using the SAMR35 as I don't need the USB functionality.  I cannot seem to change the processor type and then get the project to re-build.  Where can I find assistance with this.  There is very little documentation available for this application at all.
Thanks
#1

1 Reply Related Threads

    katlin
    New Member
    • Total Posts : 10
    • Reward points : 0
    • Joined: 2019/12/23 01:32:03
    • Location: 0
    • Status: offline
    Re: Configuring the LoRa demo code (SAMR34Xplained) to work woth the SAMR35 2020/06/05 08:50:11 (permalink)
    0
    Hi ian,
     
    SAMR34, SAMR35 Board initialization and configuration is same.
    You just need to select the Change the Device as ATSAMR35J16/17/18B and you can flash the firmware into the device.
     
    Regards,
    katlin.
     
    #2
    Jump to:
    © 2020 APG vNext Commercial Version 4.5