• AVR Freaks

Hot!Harmony V3 error when adding sys_fs

Author
Chris_Bell
New Member
  • Total Posts : 3
  • Reward points : 0
  • Joined: 2019/06/17 23:16:35
  • Location: 0
  • Status: offline
2020/03/29 06:16:27 (permalink)
0

Harmony V3 error when adding sys_fs

I am trying to create an SNMP application using the TCP/IP Application Layer Configurator and I get the following error when I try to include the file system. Below is the error and the steps that were taken to get to it.
 
MPLABX                            v5.35
XC32 compiler                   v2.4
Harmony 3                        v3.4.1
csp         v3.6.1                    bsp         v3.6.1                    mhc       v3.3.5                    net         v3.5.1                    zlib         v1.2.11
core       v3.6.1                    crypto   v3.5.0                    dev_packs          v3.6.1    CMSIS-FreeRTOS             v10.2.0
New Harmony 3 project for the PIC32MZ2048EFM144 device.
Double click the TCP/IP ApplicationLayer Configurator and then select the SNMP application in the Configuration Options.
Select ‘Yes’ to auto activate the Core (HarmonyCore) component.
Select ‘No’ to auto activate the FreeRTOS component.
Select ‘Yes’ to auto activate the TIME (sys_time) component.
Select ‘Yes’ to auto activate the CONSOLE (sys_console) component.
Select ‘Yes’ to automatically connect the
TCP/IP STACK:BASIC CONFIGURATION:tcpipStack:Core_SysConsole_Dependancy-sys_console_0:sys_console
Select ‘Yes’ to auto activate the DEBUG (sys_debug) component.
Select ‘Yes’ to automatically connect the
sys_debug:sys_debug_SYS_CONSOLE_dependancy->sys_console_0:sys_console
Select ‘Yes’ to auto activate the FILE SYSTEM (sys_fs) component.
This generates the following error
<Configuration Database>[Error]: Failed auto-connect operation. TCP/IP STACK:APPLICATION LAYER:tcpipSnmp:Snmp_TcpipFs_Dependancy->sys_fs:sys_fs is not a valid connection
 
Does anyone have any ideas on how I can include the file system without the error.
#1

1 Reply Related Threads

    freebsd
    Super Member
    • Total Posts : 157
    • Reward points : 0
    • Joined: 2011/03/07 04:15:29
    • Location: 0
    • Status: offline
    Re: Harmony V3 error when adding sys_fs 2020/03/30 20:06:52 (permalink)
    0
    There is a new Net release is coming . This issue is taken care.
    With this new core package, SYS-FS dependency with other module has been changed and this SYS-FS dependency need to be taken care with respect to Net repo also.
    #2
    Jump to:
    © 2020 APG vNext Commercial Version 4.5