• AVR Freaks

Adding a driver to H3? / Import/Export window blank in H3?

Author
photon209
New Member
  • Total Posts : 6
  • Reward points : 0
  • Joined: 2019/01/17 08:59:24
  • Location: 0
  • Status: offline
2020/03/24 08:45:22 (permalink)
0

Adding a driver to H3? / Import/Export window blank in H3?

I'm not certain this is how I should go about this, but I have the files (source/template/config etc) for the S25Fl SQI flash and I'm thinking there's a proper way to Import this into Harmony 3... is that incorrect?  Is there a different procedure?
 
So I thought that would be performed by doing an Import, but the Export/Import dialog in H3 is blank.  Is there something I need to download to get importers or exporters?
 
Cheers,
-ed
 
H3 V3.4.2
 

Product Version: MPLAB X IDE v5.15
Java: 1.8.0_181; Java HotSpot(TM) 64-Bit Server VM 25.181-b13
Runtime: Java(TM) SE Runtime Environment 1.8.0_181-b13
System: Windows 10 version 10.0 running on amd64; Cp1252; en_US (mplab)
User directory: C:\Users\efrancy.CIDRA\AppData\Roaming\mplab_ide\dev\v5.15
Cache directory: C:\Users\efrancy.CIDRA\AppData\Local\mplab_ide\Cache\dev\v5.15\var

Attached Image(s)

#1

0 Replies Related Threads

    Jump to:
    © 2020 APG vNext Commercial Version 4.5