• AVR Freaks

External Graphics Controller for S1D13517?

Author
martyray
New Member
  • Total Posts : 4
  • Reward points : 0
  • Joined: 2020/03/16 14:53:23
  • Location: 0
  • Status: offline
2020/03/21 17:47:04 (permalink)
0

External Graphics Controller for S1D13517?

Has anyone used the MHC / Graphics / External Controller as a driver for the Epson S1D13517?
 
I would be interested to learn how you configured the MHC Project Graph. I am using the Parallel Port Group to drive the Display Interface, but I am getting a compiler error:  "unknown type name 'PORT_GROUP' ".
 
Obviously this is relate to the Port Group I am using to drive the External Controller.
 
MPLAB X 5.35, XC32 v2.40, Harmony Configurator 3.4.2, PIC32MX795F-512L
 
Regards,
Marty

Attached Image(s)

#1

2 Replies Related Threads

    NKurzman
    A Guy on the Net
    • Total Posts : 18373
    • Reward points : 0
    • Joined: 2008/01/16 19:33:48
    • Location: 0
    • Status: online
    Re: External Graphics Controller for S1D13517? 2020/03/21 20:09:06 (permalink)
    0
    I used it in Harmony V1.XX but that does not help you.
    Did you check to see if there were any sample projects that use the controller. There is in Harmony 1.XX and 2.XX

    Note: It is a fairly featureless controller. No 2D accelerator or read back capabilities. It only supports block copy and layers. That And a ton of memory.
    #2
    martyray
    New Member
    • Total Posts : 4
    • Reward points : 0
    • Joined: 2020/03/16 14:53:23
    • Location: 0
    • Status: offline
    Re: External Graphics Controller for S1D13517? 2020/03/22 07:05:56 (permalink)
    0
    Thanks for the response NKurzman. Unfortunately no, I could not find a sample project for the S1D13517 for Harmony v3.xx.
     
    Still looking for help.
     
    Regards,
    Marty
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5