• AVR Freaks

Hot!Harmony v2 and S25FL Driver...

Author
tporter905
Starting Member
  • Total Posts : 35
  • Reward points : 0
  • Joined: 2010/12/06 14:13:54
  • Location: 0
  • Status: offline
2020/03/18 18:54:38 (permalink)
0

Harmony v2 and S25FL Driver...

Hi,
 
I am trying to use the Harmony S25FL driver, added the 128 and 25MBit codes, and it seems to initialize just fine. However when doing a transfer in quad serial mode it doesn't seem to work. Has anyone run into this before?
 
Thanks,
 
Tom
#1

1 Reply Related Threads

    tporter905
    Starting Member
    • Total Posts : 35
    • Reward points : 0
    • Joined: 2010/12/06 14:13:54
    • Location: 0
    • Status: offline
    Re: Harmony v2 and S25FL Driver... 2020/05/20 19:41:01 (permalink)
    0
    I got the S25FL driver working, however am running into problems where the diskio.c file doesn't get the data. Even though the buffer in that driver is coherent, and I can see the data on my logic analyzer, this driver just gets all NULL's returned...
     
    Any ideas?
     
    Thanks,
     
    Tom
    #2
    Jump to:
    © 2020 APG vNext Commercial Version 4.5