• AVR Freaks

Hot!project - wire/filament length/meter

Author
dabijja
New Member
  • Total Posts : 2
  • Reward points : 0
  • Joined: 2020/03/11 02:02:54
  • Location: 0
  • Status: offline
2020/03/17 04:48:44 (permalink)
0

project - wire/filament length/meter

Hi everybody!
 
I'm completely new to/in Microchip and I'm looking for some help in order to get the following project "live".
 
I'd like to build a (portable) device using:
1. microchip
2. reed magnetic sensor / optical encoder/magnetic encoder
3. LCD screen
4. various 3d printed and mechanical parts
5. battery operated (eventually two coin cells)
The device should be able to measure the length (either in meter or inch) of a filament/wire and display the results on an LCD/oled etc
 
I have done this project using Arduino but I think that the real "next" step is to use microchip products.
 
Any help will be appreciated.
Thank you 
 
#1

3 Replies Related Threads

    dabijja
    New Member
    • Total Posts : 2
    • Reward points : 0
    • Joined: 2020/03/11 02:02:54
    • Location: 0
    • Status: offline
    Re: project - wire/filament length/meter 2020/05/18 02:04:10 (permalink)
    0
    anybody?
    #2
    RISC
    Super Member
    • Total Posts : 5771
    • Reward points : 0
    • Status: offline
    Re: project - wire/filament length/meter 2020/05/18 02:55:15 (permalink)
    +2 (2)
    Hi,
    If you already implemented this using Arduino, you probably know what is needed in your system and in the microcontroller. To select these components there are a couple of "selector tools" :
    MAPS   and TREELINK
    If you post a block diagram of your system with more details you will probably get more help here...
    What kind of LCD (spec ?)?
    Which technique have you used to measure filament => peripheral needed in the microcontroller ?
    etc...
    Regards
    #3
    crosland
    Super Member
    • Total Posts : 2009
    • Reward points : 0
    • Joined: 2005/05/10 10:55:05
    • Location: Warks, UK
    • Status: offline
    Re: project - wire/filament length/meter 2020/05/18 02:58:53 (permalink)
    0
    I think you need to ask more specific questions. What are you struggling with?
    #4
    Jump to:
    © 2020 APG vNext Commercial Version 4.5