• AVR Freaks

Hot!PIC32MK GP dev board DM32006: CAN Bus example

Author
vlele
New Member
  • Total Posts : 4
  • Reward points : 0
  • Joined: 2018/07/19 08:57:15
  • Location: 0
  • Status: offline
2020/02/26 02:55:10 (permalink)
0

PIC32MK GP dev board DM32006: CAN Bus example

Hi,
 
I just bought the development kit DM32006.
 
I am unable to find the example code for CAN peripheral.
I am trying to send CAN message .
 
Thanks.
#1

6 Replies Related Threads

    NKurzman
    A Guy on the Net
    • Total Posts : 18392
    • Reward points : 0
    • Joined: 2008/01/16 19:33:48
    • Location: 0
    • Status: online
    Re: PIC32MK GP dev board DM32006: CAN Bus example 2020/02/26 10:09:34 (permalink)
    0
    DM32006 does not show up as a valid part number.  Is it complete
     
    For All the bigger PIC32 chips Harmony will have the Examples.  If they are missing in V3.XX try V2.06
    #2
    pcbbc
    Super Member
    • Total Posts : 1637
    • Reward points : 0
    • Joined: 2014/03/27 07:04:41
    • Location: 0
    • Status: offline
    Re: PIC32MK GP dev board DM32006: CAN Bus example 2020/02/26 10:26:45 (permalink)
    0
    Plus this is the 8 bit forum.
    You'd probably be better off seeking help in either the Communications Forum or one of the 32-Bit Microcontrollers Forums. grin: grin
    #3
    vlele
    New Member
    • Total Posts : 4
    • Reward points : 0
    • Joined: 2018/07/19 08:57:15
    • Location: 0
    • Status: offline
    Re: PIC32MK GP dev board DM32006: CAN Bus example 2020/02/26 10:33:40 (permalink)
    0
    https://www.microchip.com/DevelopmentTools/ProductDetails/PartNO/DM320006
    #4
    vlele
    New Member
    • Total Posts : 4
    • Reward points : 0
    • Joined: 2018/07/19 08:57:15
    • Location: 0
    • Status: offline
    Re: PIC32MK GP dev board DM32006: CAN Bus example 2020/02/26 10:34:48 (permalink)
    0
    How can I change forum to 32bit?
    #5
    Jim Nickerson
    User 452
    • Total Posts : 6566
    • Reward points : 0
    • Joined: 2003/11/07 12:35:10
    • Location: San Diego, CA
    • Status: offline
    Re: PIC32MK GP dev board DM32006: CAN Bus example 2020/02/26 10:39:28 (permalink)
    +1 (1)
    start a new post in the 32 bit forum
    come back here and place a link to new post in 32 bit forum
    your original post is missing a "0" in the part number
    #6
    NKurzman
    A Guy on the Net
    • Total Posts : 18392
    • Reward points : 0
    • Joined: 2008/01/16 19:33:48
    • Location: 0
    • Status: online
    Re: PIC32MK GP dev board DM32006: CAN Bus example 2020/02/26 14:16:21 (permalink)
    0
    DM320006 is a discontinued board for the PIC32MZ EC CPU.  One NOT Recommended for new designs. 
    Is that what you are planning to use?  An where did you Just Buy it?  You may need to back up to Harmony V1.11 (or earlier) for that PIC
    #7
    Jump to:
    © 2020 APG vNext Commercial Version 4.5