• AVR Freaks

Hot!Text Via LAN

Author
Designer
Super Member
  • Total Posts : 519
  • Reward points : 0
  • Joined: 2007/11/20 20:28:41
  • Location: 0
  • Status: offline
2020/02/26 02:53:36 (permalink)
5 (1)

Text Via LAN

I have to build IP based wired alarm system. I have one master & 5 slaves.Master has 5 push buttons.
 
What I want to do is to use existing LAN infrastructure (cabling) & plug my devices to that network.when master press the button the corresponding slave device must turn on the alarm. Thats it.
 
Note: The existing LAN infrastructure is occupying PCs, Printers, Internet etc... I want to plug my devices to this network.
 
Is there any method to do this? PIC16F solution will be better...!! Any modules I can purchase as well.
#1

2 Replies Related Threads

    NKurzman
    A Guy on the Net
    • Total Posts : 18848
    • Reward points : 0
    • Joined: 2008/01/16 19:33:48
    • Location: 0
    • Status: offline
    Re: Text Via LAN 2020/02/26 06:46:42 (permalink)
    0
    You could use WIZNet modules. Or something similar.
    You would need bigger PICs if you want to run the stack on the chip.
    #2
    LdB_ECM
    Super Member
    • Total Posts : 401
    • Reward points : 0
    • Joined: 2019/04/16 22:01:25
    • Location: 0
    • Status: offline
    Re: Text Via LAN 2020/02/26 07:19:52 (permalink)
    +1 (1)
    Telnet protocol is the easiest usually on Port23  ... the exchange is normal text
     
    All you need is to have a socket library for the device. The device is typically the client and it opens a telnet session to the server via a fixed IP (you can usually set it).
     
    If you want to see what it looks like download a telnet client like putty (https://www.putty.org/) then hit any of the public telnet servers
    try
    scn.org     .... login as visitor
     
    Real security systems which use the internet us SSH in which the data is encrypted and have certificates. So it's just a complex mangling of the text data the unit and server exchange.
     
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5