• AVR Freaks

Hot!MA330046 dsPIC33CH512MP508 PIM demo project files?

Author
Sobottech
Super Member
  • Total Posts : 280
  • Reward points : 0
  • Joined: 2015/12/02 03:32:17
  • Location: 0
  • Status: offline
2020/02/24 07:35:59 (permalink)
5 (1)

MA330046 dsPIC33CH512MP508 PIM demo project files?

Hi,
checking the dsPIC33CH512MP508 General Purpose PIM Info Sheet for the MA330046, there sould be a demo project.
"This demo project provides a basic demonstration of how to use both the Master and Slave cores within the dsPIC33CH512MP508, and how to use the Master/Slave core interface for sending data between the cores. The master"
 
But there is no demo project.
Also checking dsPIC33CH512MP508, there is not this mentioned demo project.
 
On microchipdeveloper there is an other project/help.
 
But where to get the source code from the dsPIC33CH512MP508 General Purpose Plug-In Module (PIM) .pdf-file?
 
[sorry, inserted links, but received an error message from the forum]
#1

2 Replies Related Threads

    davekw7x
    Entropy++
    • Total Posts : 1849
    • Reward points : 0
    • Joined: 2012/01/16 12:01:07
    • Location: Second star on the right, straight on till morning
    • Status: offline
    Re: MA330046 dsPIC33CH512MP508 PIM demo project files? 2020/02/24 16:33:21 (permalink)
    0
    Sobottech
    ...source code from the dsPIC33CH512MP508 General Purpose Plug-In Module (PIM) .pdf-file?

    Try this:
    Go to the Explorer 16/32 DevelopmentTools Documents and Software page:
    https://www.microchip.com...ductDetails/DM240001-2

    Click on the Explorer 16/32 Board Demo Code link and download
    explorer16_demo_2019_06_07.zip

    This has an MPLABX project for the dsPIC33CH512MP508 PIM demo and demo projects for beaucoup other PIMS.

    Regards,

    Dave

    Footnote
    It's Mardi Gras:
    Laissez les bon temp rouller!


    post edited by davekw7x - 2020/02/24 16:40:52

    Sometimes I just can't help myself...
    #2
    Sobottech
    Super Member
    • Total Posts : 280
    • Reward points : 0
    • Joined: 2015/12/02 03:32:17
    • Location: 0
    • Status: offline
    Re: MA330046 dsPIC33CH512MP508 PIM demo project files? 2020/03/04 01:10:52 (permalink)
    0
    Ah, yes.
    Thank you very much.
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5