• AVR Freaks

AnsweredHot!Harmony V3 Bad SYSCLK Calculation

Author
Codewizards
New Member
  • Total Posts : 2
  • Reward points : 0
  • Joined: 2020/02/03 02:36:16
  • Location: 0
  • Status: offline
2020/02/19 12:11:18 (permalink)
0

Harmony V3 Bad SYSCLK Calculation

Hi,
The configurator calculating wrong SYSCLK.
I cannot get 80Mhz SYSCLK only 72Mhz. The input clk is 8Mhz crystal and I use the standard PLL configuration (DIV_2 and MUL_20), but the configurator allways calculating 72Mhz which is wrong.
Even worse the Clock configurator tool do the same and complains that HS oscillator must be between 10-25 Mhz which is wrong, and don't want to use MUL_20 only MUL_18 which results in 72Mhz.
 
Is there any reason doing this, or it is a simple bug?
 
Regards
 
#1
nigelwright7557
Super Member
  • Total Posts : 369
  • Reward points : 0
  • Joined: 2006/11/06 08:15:51
  • Location: 0
  • Status: offline
Re: Harmony V3 Bad SYSCLK Calculation 2020/02/19 15:46:36 (permalink)
0
I suspect 72MHz is max frequency of processor hence it wont go any higher.
 
#2
arpananand
Super Member
  • Total Posts : 453
  • Reward points : 0
  • Joined: 2009/11/18 04:35:42
  • Location: 0
  • Status: offline
Re: Harmony V3 Bad SYSCLK Calculation 2020/02/19 19:18:57 (permalink)
0
which device are you using?
#3
Codewizards
New Member
  • Total Posts : 2
  • Reward points : 0
  • Joined: 2020/02/03 02:36:16
  • Location: 0
  • Status: offline
Re: Harmony V3 Bad SYSCLK Calculation 2020/02/20 01:11:15 (permalink)
0
Hi,
 
It is a PIC32MX795F512L which is running on 80Mhz max and we use it successfully over many years in multiple products.
Right now I just tried to migrate one of our project into Harmony 3 and start playing with this, and realised tht H3 caps the device speed at 72Mhz whatever I do.
 
Best Regards
 
 
 
#4
arpananand
Super Member
  • Total Posts : 453
  • Reward points : 0
  • Joined: 2009/11/18 04:35:42
  • Location: 0
  • Status: offline
Re: Harmony V3 Bad SYSCLK Calculation 2020/02/20 03:19:38 (permalink) ☼ Best Answerby Codewizards 2020/02/20 03:27:53
0
its a bug which will be fixed in next release. for now you can configure multiplier value in  DEVCFG2 device configuration tree structure and proceed. 
#5
Jump to:
© 2020 APG vNext Commercial Version 4.5