• AVR Freaks

Duplicate external apps addition to existing project Harmony V3Duplicate

Author
FlutterBy
New Member
  • Total Posts : 9
  • Reward points : 0
  • Joined: 2019/11/13 05:08:11
  • Location: 0
  • Status: offline
2020/02/13 03:18:23 (permalink)
0

Duplicate external apps addition to existing project Harmony V3Duplicate

Hi,
Using Harmony v3.4.1
XC32 V2.30
MPLAB IDE 5.30
Project tcpip_tcp_client pic32mx_eth_sk2.X converted to UDP as there is not one for UDP on the MX yet
Ethernet Starter Kit 2, LAN8740 PHY Daughter Board, pic32mx795f512l

I already have an app written on a PIC32, I just want it to be listening to a certain UDP Port waiting for data to coming in, it won't ack anything.
 
Where do I place the app? is it in main?? do I update the UDP.c or the existing app.c or just include the socket setup as par of myapp?
 
Thanks in advance
post edited by FlutterBy - 2020/02/14 00:38:49
#1

1 Reply Related Threads

    ric
    Super Member
    • Total Posts : 25632
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: offline
    Re: external apps addition to existing project Harmony V3 2020/02/13 12:11:53 (permalink)

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #2
    Jump to:
    © 2020 APG vNext Commercial Version 4.5