• AVR Freaks

Hot!Harmony3 + PIC32MZ starter kit + WINC1500 code generator error

Author
RobinDeleener
New Member
  • Total Posts : 1
  • Reward points : 0
  • Joined: 2020/02/10 07:56:03
  • Location: 0
  • Status: offline
2020/02/13 03:10:54 (permalink)
0

Harmony3 + PIC32MZ starter kit + WINC1500 code generator error

Dear all,
 
I have a PIC32MZ starterkit (PIC32MZ2048ECM144) mounted via the '168pin to 132pin starter kit adapter' on the 'Starter Kit I/O expansions board' where I plugged in the 'WINC1500 PicTail daughter board'.
I already configured in harmony the TCP/IP stack with the LAN7840 driver which is fully working.
Now I want to add to the stack the WINC1500. I added the WINC1500 driver in harmony, the SPI peripheral and SPI driver.
 
https://www.dropbox.com/s/sej2iuwnf42iycb/HarmonyConfig.PNG?dl=0

 
Now when I want to generate the code, Harmony is giving the follwing error:
 
https://www.dropbox.com/s/nccs2tu7lqc4cf9/HarmonyError.PNG?dl=0

 
The Harmony examples of WINC1500 only have code for the SAM family. The Harmony configurator for the WINCdriver when selecting a SAM device gives a checkbox to choose the interrupt source which is not present when selecting PIC32MZ as device. The PIC32MZ doesn't have the EIC so that's probably why.
 
https://www.dropbox.com/s/2fbeyrt9lphijjr/HarmonyWINCdriver.png?dl=0

 
I geuss that's where the error is coming from. But how can I resolve this error?
 
(I already tried to adapt the system_config.h.ftl file by commenting the '#if'. Then it can generate a code but comiling the project gives errors).
 
Thanks in advance for your help!
 
#1

2 Replies Related Threads

    donald
    New Member
    • Total Posts : 3
    • Reward points : 0
    • Joined: 2010/09/01 23:01:26
    • Location: 0
    • Status: offline
    Re: Harmony3 + PIC32MZ starter kit + WINC1500 code generator error 2020/02/18 20:45:48 (permalink)
    0
    I have same problem.
    WINCdriver cannot assign inturrupt source in GUI.
    We can do nothing until update release...PLZ
     
     
    #2
    donald
    New Member
    • Total Posts : 3
    • Reward points : 0
    • Joined: 2010/09/01 23:01:26
    • Location: 0
    • Status: offline
    Re: Harmony3 + PIC32MZ starter kit + WINC1500 code generator error 2020/05/21 03:49:01 (permalink)
    0
    Same problem here!!!
    How long do we have to wait!!
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5