• AVR Freaks

Duplicate external apps addition to existing project Harmony V3 Duplicate

Author
FlutterBy
New Member
  • Total Posts : 7
  • Reward points : 0
  • Joined: 2019/11/13 05:08:11
  • Location: 0
  • Status: offline
2020/02/13 02:49:34 (permalink)
0

Duplicate external apps addition to existing project Harmony V3 Duplicate

Hi,
Using Harmony v3.4.1
XC32 V2.30
MPLAB IDE 5.30
Project tcpip_tcp_client pic32mx_eth_sk2.X converted to UDP as there is not one for UDP on the MX yet
Ethernet Starter Kit 2, LAN8740 PHY Daughter Board, pic32mx795f512l
 
I already have an app written on a PIC32, I just want it to be listening to a certain UDP Port waiting for data to coming in, it won't ack anything.
 
Where do I place the app? is it in main?? do I update the UDP.c or the existing app.c or just include the socket setup as par of myapp?
 
Thanks in advance
post edited by FlutterBy - 2020/02/14 00:39:36
#1

2 Replies Related Threads

    ric
    Super Member
    • Total Posts : 25555
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: online
    Re: external apps addition to existing project Harmony V3 2020/02/13 12:11:19 (permalink)

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #2
    PStechPaul
    Super Member
    • Total Posts : 2502
    • Reward points : 0
    • Joined: 2006/06/27 16:11:32
    • Location: Cockeysville, MD, USA
    • Status: online
    Re: external apps addition to existing project Harmony V3 2020/02/13 12:51:35 (permalink)
    0
    The OP should change the title of three of these duplicate posts to "duplicate", "ignore", or "closed". Then someone can reply to the remaining post. This is probably caused by the dysfunctional and crippled forum software not providing adequate feedback to the poster. And reasonably smart professional commercial forum software should detect and disallow duplicate posts. I thought they had already done that to stop the spambots that have occasionally attacked the forum, which seems to have been written and maintained by code monkeys...

     
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5