• AVR Freaks

Hot!Problems with mtouch configuration

Author
Aybood
New Member
  • Total Posts : 21
  • Reward points : 0
  • Joined: 2017/11/16 07:27:47
  • Location: 0
  • Status: offline
2020/02/04 04:15:42 (permalink)
0

Problems with mtouch configuration

Hi,
I want to configure my nano curiosity (pic16f18446 with internal ADC2)  to work with cap touch buttons using mtoch library, I followed the provided guides from microchip but nothing works, I just want to know if should I put the ADC2 in MCC or just the mtouch? 
 
I checked the library of mtouch and i found that the mtouch initialize the ADC2.
If anyone had the same problem to configure right the touch buttons, can you share your experience, please?
 
In attachments, you can find 2 photos of the 2 configurations above mentioned, can anyone tell me if there is something wrong?
 
Thanks
 

Attached Image(s)

#1
XiangGao
Senior Member
  • Total Posts : 57
  • Reward points : 0
  • Joined: 2016/07/07 15:54:59
  • Location: 0
  • Status: offline
Re: Problems with mtouch configuration 2020/03/13 09:08:25 (permalink)
0
Hello, 
 
You will not need to use ADC, the mTouch library will initialize the ADC.
 
Please follow the guide here.https://microchipdeveloper.com/touch:lowcost-mtouch-kit
 
 
#2
Jump to:
© 2020 APG vNext Commercial Version 4.5