• AVR Freaks

Hot!Harmony 2.06 draw surface widget

Author
hmpmcp
New Member
  • Total Posts : 7
  • Reward points : 0
  • Joined: 2016/04/29 01:09:05
  • Location: 0
  • Status: offline
2020/01/28 02:13:38 (permalink)
0

Harmony 2.06 draw surface widget

Hello, are there any documentation about the draw surface widget? With try and error (not really efficient) I can draw somewhat with the GFX_DrawRect function. I can draw a line with the GFX_DrawLine function, but the parameters have to be constants. The GFX_DrawCircle function let the program go to the Nirwana. Any ideas? Best regards Hartmut Leue H2.06, MPLAB 5.10, XC32 V2.30
#1

0 Replies Related Threads

    Jump to:
    © 2020 APG vNext Commercial Version 4.5