• AVR Freaks

Hot!Thread for suggestions for the next release of MPLAB IDE?

Author
kaamil1984
Junior Member
  • Total Posts : 40
  • Reward points : 0
  • Joined: 2014/05/01 14:02:25
  • Location: Chair at the desk in my workshop ;)
  • Status: offline
2020/01/27 05:44:25 (permalink)
5 (1)

Thread for suggestions for the next release of MPLAB IDE?

Hi guys,
 
I saw that MCC has "Suggestions for the next release of MPLAB® Code Configurator" thread on forum.
 
Can we have "Suggestions for the next release of MPLAB® IDE"?
 
I would like to suggest one or more little things from other IDE's.
 
Suggestion for example:
 
LINK TO OUTPUT DIRECTORY IN COMPILER OUTPUT WINDOW
 
In the output window, after I build the project I see message like this:
Memory Summary:
Program space used C88Bh ( 51339) of 20000h bytes ( 39.2%)
Data space used A6Eh ( 2670) of DEAh bytes ( 75.0%)
Configuration bits used 6h ( 6) of 6h words (100.0%)
EEPROM space used 0h ( 0) of 400h bytes ( 0.0%)
ID Location space used 10h ( 16) of 10h bytes (100.0%)
Data stack space used 0h ( 0) of 358h bytes ( 0.0%)
 
make[2]: Leaving directory 'C:/Users/KA/Documents/Work/GS/Projects/24ses-expanders-s1'
make[1]: Leaving directory 'C:/Users/KA/Documents/Work/GS/Projects/24ses-expanders-s1'
 
BUILD SUCCESSFUL (total time: 39s)
Loading code from C:/Users/KA/Documents/Work/GS/Projects/24ses-expanders-s1/dist/default/production/24ses-expanders-s1.production.hex...
Loading completed
After this (or somewhere in the middle) there could be a clickable link that opens directory where hex file is located. Maybe something like this:
 
        Click to open dist directory:
        C:/Users/KA/Documents/Work/GS/Projects/24ses-expanders-s1/dist/default/production/
 
This is idea from IntelliJ IDE (Java development IDE) and I found this very productive.
 
---
Have a nice day
Kamil
 
#1

0 Replies Related Threads

    Jump to:
    © 2020 APG vNext Commercial Version 4.5