• AVR Freaks

Hot!Why can't I select optimisation level 3 even if I have the PRO compiler subscription?

Author
AndersG
Senior Member
  • Total Posts : 179
  • Reward points : 0
  • Joined: 2008/08/05 04:51:24
  • Location: 0
  • Status: offline
2020/01/26 02:39:34 (permalink)
0

Why can't I select optimisation level 3 even if I have the PRO compiler subscription?

Ie, 2 works, but 3 gives:
The current license does not permit the selected optimization level, using optimization level 2
Could this be the issue?
 
C:\Program Files (x86)\Microchip\xc8\v2.10\bin>xclm -status
Microchip XC License Manager Version: 2.26
License Path: C:\ProgramData\Microchip\xclm/license/\
Product: rlm_roam Type: Workstation Version: 1.0 Mode: ?
How do I fix this? It seems that I have several "renewed" files in my license folder, but nothing more recent than dec 20 2019
 
Asking here in case I have done something stupid, but have also fired away an email to swlicensing at Microchip.
#1

0 Replies Related Threads

    Jump to:
    © 2020 APG vNext Commercial Version 4.5