• AVR Freaks

Hot!Error in MPLAB X IDE V5.20?

Author
Theo
Starting Member
  • Total Posts : 42
  • Reward points : 0
  • Joined: 2019/05/04 18:51:24
  • Location: 0
  • Status: offline
2020/01/24 10:44:02 (permalink)
0

Error in MPLAB X IDE V5.20?

Hi,
Looking at the SFRs in MPLAB (using PIC16F18326) under NCO (Numerically Controlled Oscillator) CLC1CON is shown in stead of NCO1CON. Confusing.
 
Should I report this somewhere?
#1

4 Replies Related Threads

    NKurzman
    A Guy on the Net
    • Total Posts : 18266
    • Reward points : 0
    • Joined: 2008/01/16 19:33:48
    • Location: 0
    • Status: online
    Re: Error in MPLAB X IDE V5.20? 2020/01/24 10:49:32 (permalink)
    +1 (1)
    You Should if it is also in V5.30 (the current Version)
     
    #2
    Theo
    Starting Member
    • Total Posts : 42
    • Reward points : 0
    • Joined: 2019/05/04 18:51:24
    • Location: 0
    • Status: offline
    Re: Error in MPLAB X IDE V5.20? 2020/01/24 11:43:52 (permalink)
    0
    Yes, the problem still exists in V5.30.
     
    Where exactly should I report this? Open a ticket?
    #3
    NKurzman
    A Guy on the Net
    • Total Posts : 18266
    • Reward points : 0
    • Joined: 2008/01/16 19:33:48
    • Location: 0
    • Status: online
    Re: Error in MPLAB X IDE V5.20? 2020/01/24 12:21:45 (permalink)
    +1 (1)
    Yes You would Open a Support Ticket.
    #4
    ric
    Super Member
    • Total Posts : 25592
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: online
    Re: Error in MPLAB X IDE V5.20? 2020/01/24 13:40:05 (permalink)
    0
    Theo de Kok
    Looking at the SFRs in MPLAB

    I'm sure you mean MPLABX, not MPLAB.
    Many people still use MPLAB, so it's important to note the correct one.
     

    (using PIC16F18326) under NCO (Numerically Controlled Oscillator) CLC1CON is shown in stead of NCO1CON.

    Where exactly are you looking in MPLABX?
    Is this actually inside MCC?
     
     

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #5
    Jump to:
    © 2020 APG vNext Commercial Version 4.5