• AVR Freaks

Hot!SD card mount fail PIC32mz2048efm144

Author
jigarpatel588
New Member
  • Total Posts : 3
  • Reward points : 0
  • Joined: 2020/01/21 13:08:30
  • Location: 0
  • Status: offline
2020/01/22 11:49:58 (permalink)
0

SD card mount fail PIC32mz2048efm144

I am interfacing SDHC 8gb card with PIC32mz2048efm144.
create code using harmony v3. 
always get fail status from SYS_FS_Mount function.
did all the same configuration as per https://microchipdeveloper.com/harmony3:audio-player-lab2#Step6_anchor
 
also on microchip developer link has sample code for harmony v3 but not able to download.
 
#1

4 Replies Related Threads

    SyeT
    Starting Member
    • Total Posts : 52
    • Reward points : 0
    • Joined: 2012/07/24 00:38:10
    • Location: 0
    • Status: offline
    Re: SD card mount fail PIC32mz2048efm144 2020/01/26 21:19:11 (permalink)
    0
    Hi,
     
    Looks like the link for the solution is broken. I have complained to fix it. Will update once it is fixed.
     
    Thanks.
     
    Best Regards,
    SyeT
    #2
    NKurzman
    A Guy on the Net
    • Total Posts : 18245
    • Reward points : 0
    • Joined: 2008/01/16 19:33:48
    • Location: 0
    • Status: offline
    Re: SD card mount fail PIC32mz2048efm144 2020/01/26 22:53:49 (permalink)
    0
    The card is formatted for FAT32.
    #3
    jigarpatel588
    New Member
    • Total Posts : 3
    • Reward points : 0
    • Joined: 2020/01/21 13:08:30
    • Location: 0
    • Status: offline
    Re: SD card mount fail PIC32mz2048efm144 2020/01/27 07:03:24 (permalink)
    0
    Yes card is formatted for FAT32
    #4
    SyeT
    Starting Member
    • Total Posts : 52
    • Reward points : 0
    • Joined: 2012/07/24 00:38:10
    • Location: 0
    • Status: offline
    Re: SD card mount fail PIC32mz2048efm144 2020/01/29 19:50:27 (permalink)
    0
    Hi,
     
    Please note the download link on the developer help page https://microchipdeveloper.com/harmony3:audio-player
     
    https://microchiptechnology-my.sharepoint.com/:u:/g/personal/kent_myers_microchip_com/EeM0yIfnwKxJt1ZWs7s36w4BbEkld7XlUx5JIJmpPD_wRg?e=4%3aw52Niy&at=9
     
    is now working. Please refer to the solution for Lab2.
     
    Thanks.
     
    Best Regards,
    Syed
    #5
    Jump to:
    © 2020 APG vNext Commercial Version 4.5