• AVR Freaks

Helpful ReplyHot!PIC24FJ256GA106 and PIC24FJ64GA102 : math library

Author
nrobin
New Member
  • Total Posts : 11
  • Reward points : 0
  • Joined: 2019/11/21 04:03:23
  • Location: 0
  • Status: offline
2020/01/21 07:41:54 (permalink)
0

PIC24FJ256GA106 and PIC24FJ64GA102 : math library

Hi,
 
i use inclination sensor for my application. In order to determine angle, i would like to use asin() function.
In which library is defined this asin() function ?
 
Thank you
#1
NKurzman
A Guy on the Net
  • Total Posts : 18266
  • Reward points : 0
  • Joined: 2008/01/16 19:33:48
  • Location: 0
  • Status: offline
Re: PIC24FJ256GA106 and PIC24FJ64GA102 : math library 2020/01/21 07:56:35 (permalink) ☄ Helpfulby nrobin 2020/01/21 08:12:03
0
Did you try math.h?
#2
nrobin
New Member
  • Total Posts : 11
  • Reward points : 0
  • Joined: 2019/11/21 04:03:23
  • Location: 0
  • Status: offline
Re: PIC24FJ256GA106 and PIC24FJ64GA102 : math library 2020/01/21 08:13:13 (permalink)
0
thank you. It is ok now.
#3
ric
Super Member
  • Total Posts : 25592
  • Reward points : 0
  • Joined: 2003/11/07 12:41:26
  • Location: Australia, Melbourne
  • Status: online
Re: PIC24FJ256GA106 and PIC24FJ64GA102 : math library 2020/01/21 12:24:05 (permalink)
5 (1)
In future, you can just look in:
C:\Program Files (x86)\Microchip\xc16\v1.33\docs\16-Bit_Language_Tools_Libraries_Manual.pdf
(Update the version number in the path to suit your copy of XC16)
 

I also post at: PicForum
Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
NEW USERS: Posting images, links and code - workaround for restrictions.
To get a useful answer, always state which PIC you are using!
#4
Jump to:
© 2020 APG vNext Commercial Version 4.5