• AVR Freaks

Hot!RN4020 disconnects in Windows 10

Author
Sh@dow
Starting Member
  • Total Posts : 62
  • Reward points : 0
  • Joined: 2009/04/08 11:49:15
  • Location: 0
  • Status: offline
2020/01/20 10:59:06 (permalink)
0

RN4020 disconnects in Windows 10

hi all
I am using RN4020 to connect with windows 10 pc.
Pc supports BTLE as it has "Microsoft Bluetooth LE Enumerator" in device manager.
Pc find the module. I am doing pairing. After "Connected" message appear in terminal "Disconnected" message comes.
Why does that happen? I guess because no services selected after pairing is done but not sure.
 
#1

1 Reply Related Threads

    Sh@dow
    Starting Member
    • Total Posts : 62
    • Reward points : 0
    • Joined: 2009/04/08 11:49:15
    • Location: 0
    • Status: offline
    Re: RN4020 disconnects in Windows 10 2020/01/21 08:57:23 (permalink)
    0
    There is some progress.
    I have downloaded Bluetooth LE Explorer and connected to RN4020. It seems ok now.
    #2
    Jump to:
    © 2020 APG vNext Commercial Version 4.5